public static class ExtractFaceBuilder.FeatureOptionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ONE_FEATURE_FOR_ALL_BODIES
An option to create one extracted or linked body feature for all selected bodies as body collector
|
static int |
_SEPARATE_FEATURE_FOR_EACH_BODY
An option to create a separate extracted or linked body feature per single body
|
static ExtractFaceBuilder.FeatureOptionType |
ONE_FEATURE_FOR_ALL_BODIES
An option to create one extracted or linked body feature for all selected bodies as body collector
|
static ExtractFaceBuilder.FeatureOptionType |
SEPARATE_FEATURE_FOR_EACH_BODY
An option to create a separate extracted or linked body feature per single body
|
Modifier and Type | Method and Description |
---|---|
static ExtractFaceBuilder.FeatureOptionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtractFaceBuilder.FeatureOptionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtractFaceBuilder.FeatureOptionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ExtractFaceBuilder.FeatureOptionType ONE_FEATURE_FOR_ALL_BODIES
public static final ExtractFaceBuilder.FeatureOptionType SEPARATE_FEATURE_FOR_EACH_BODY
public static final int _ONE_FEATURE_FOR_ALL_BODIES
public static final int _SEPARATE_FEATURE_FOR_EACH_BODY
public static ExtractFaceBuilder.FeatureOptionType valueOf(int value)
public static ExtractFaceBuilder.FeatureOptionType valueOf(String name)
public static ExtractFaceBuilder.FeatureOptionType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.