Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ExtractFaceBuilder.FeatureOptionType |
ExtractFaceBuilder.FeatureOptionType.ONE_FEATURE_FOR_ALL_BODIES
An option to create one extracted or linked body feature for all selected bodies as body collector
|
static ExtractFaceBuilder.FeatureOptionType |
ExtractFaceBuilder.FeatureOptionType.SEPARATE_FEATURE_FOR_EACH_BODY
An option to create a separate extracted or linked body feature per single body
|
Modifier and Type | Method and Description |
---|---|
ExtractFaceBuilder.FeatureOptionType |
ExtractFaceBuilder.featureOption()
Returns the feature option type
License requirements: None. |
static ExtractFaceBuilder.FeatureOptionType |
ExtractFaceBuilder.FeatureOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtractFaceBuilder.FeatureOptionType |
ExtractFaceBuilder.FeatureOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtractFaceBuilder.FeatureOptionType[] |
ExtractFaceBuilder.FeatureOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExtractFaceBuilder.setFeatureOption(ExtractFaceBuilder.FeatureOptionType featureOptionType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.