public static class BridgeCurveBuilder.SurfaceDirectionTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ISO_U
bridge direction takes u-isoparametric direction
of the base surface at the selected point
|
static int |
_ISO_V
bridge direction takes v-isoparametric direction
of the base surface at the selected point
|
static int |
_SECTIONAL
bridge direction takes non-isoparametric direction
of the base surface at the selected point
|
static BridgeCurveBuilder.SurfaceDirectionTypes |
ISO_U
bridge direction takes u-isoparametric direction
of the base surface at the selected point
|
static BridgeCurveBuilder.SurfaceDirectionTypes |
ISO_V
bridge direction takes v-isoparametric direction
of the base surface at the selected point
|
static BridgeCurveBuilder.SurfaceDirectionTypes |
SECTIONAL
bridge direction takes non-isoparametric direction
of the base surface at the selected point
|
Modifier and Type | Method and Description |
---|---|
static BridgeCurveBuilder.SurfaceDirectionTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.SurfaceDirectionTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.SurfaceDirectionTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final BridgeCurveBuilder.SurfaceDirectionTypes SECTIONAL
public static final BridgeCurveBuilder.SurfaceDirectionTypes ISO_U
public static final BridgeCurveBuilder.SurfaceDirectionTypes ISO_V
public static final int _SECTIONAL
public static final int _ISO_U
public static final int _ISO_V
public static BridgeCurveBuilder.SurfaceDirectionTypes valueOf(int value)
public static BridgeCurveBuilder.SurfaceDirectionTypes valueOf(String name)
public static BridgeCurveBuilder.SurfaceDirectionTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.