public static class BridgeCurveBuilder.ShapeControlTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONIC
conic parameter
|
static int |
_END_POINT
end point conditions
|
static int |
_PEAK_POINT
peak point conditions
|
static int |
_SHAPE_CURVE
shape curve
|
static BridgeCurveBuilder.ShapeControlTypes |
CONIC
conic parameter
|
static BridgeCurveBuilder.ShapeControlTypes |
END_POINT
end point conditions
|
static BridgeCurveBuilder.ShapeControlTypes |
PEAK_POINT
peak point conditions
|
static BridgeCurveBuilder.ShapeControlTypes |
SHAPE_CURVE
shape curve
|
Modifier and Type | Method and Description |
---|---|
static BridgeCurveBuilder.ShapeControlTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.ShapeControlTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.ShapeControlTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final BridgeCurveBuilder.ShapeControlTypes END_POINT
public static final BridgeCurveBuilder.ShapeControlTypes PEAK_POINT
public static final BridgeCurveBuilder.ShapeControlTypes CONIC
public static final BridgeCurveBuilder.ShapeControlTypes SHAPE_CURVE
public static final int _END_POINT
public static final int _PEAK_POINT
public static final int _CONIC
public static final int _SHAPE_CURVE
public static BridgeCurveBuilder.ShapeControlTypes valueOf(int value)
public static BridgeCurveBuilder.ShapeControlTypes valueOf(String name)
public static BridgeCurveBuilder.ShapeControlTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.