public static class AestheticFaceBlendBuilder.AlignmentType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ROLLING_BALL
Rolling Ball option will align the sections at contact point.
|
static int |
_SPINE_CURVE
Spine Curve option will align the sections based on a string of curves.
|
static int |
_VECTOR
Vector option will align the sections based on the vector
|
static AestheticFaceBlendBuilder.AlignmentType |
ROLLING_BALL
Rolling Ball option will align the sections at contact point.
|
static AestheticFaceBlendBuilder.AlignmentType |
SPINE_CURVE
Spine Curve option will align the sections based on a string of curves.
|
static AestheticFaceBlendBuilder.AlignmentType |
VECTOR
Vector option will align the sections based on the vector
|
Modifier and Type | Method and Description |
---|---|
static AestheticFaceBlendBuilder.AlignmentType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AestheticFaceBlendBuilder.AlignmentType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AestheticFaceBlendBuilder.AlignmentType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AestheticFaceBlendBuilder.AlignmentType ROLLING_BALL
public static final AestheticFaceBlendBuilder.AlignmentType SPINE_CURVE
public static final AestheticFaceBlendBuilder.AlignmentType VECTOR
public static final int _ROLLING_BALL
public static final int _SPINE_CURVE
public static final int _VECTOR
public static AestheticFaceBlendBuilder.AlignmentType valueOf(int value)
public static AestheticFaceBlendBuilder.AlignmentType valueOf(String name)
public static AestheticFaceBlendBuilder.AlignmentType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.