Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AestheticFaceBlendBuilder.AlignmentType |
AestheticFaceBlendBuilder.AlignmentType.ROLLING_BALL
Rolling Ball option will align the sections at contact point.
|
static AestheticFaceBlendBuilder.AlignmentType |
AestheticFaceBlendBuilder.AlignmentType.SPINE_CURVE
Spine Curve option will align the sections based on a string of curves.
|
static AestheticFaceBlendBuilder.AlignmentType |
AestheticFaceBlendBuilder.AlignmentType.VECTOR
Vector option will align the sections based on the vector
|
Modifier and Type | Method and Description |
---|---|
AestheticFaceBlendBuilder.AlignmentType |
AestheticFaceBlendBuilder.alignmentOption()
Returns the alignment option
License requirements: None. |
static AestheticFaceBlendBuilder.AlignmentType |
AestheticFaceBlendBuilder.AlignmentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AestheticFaceBlendBuilder.AlignmentType |
AestheticFaceBlendBuilder.AlignmentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AestheticFaceBlendBuilder.AlignmentType[] |
AestheticFaceBlendBuilder.AlignmentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AestheticFaceBlendBuilder.setAlignmentOption(AestheticFaceBlendBuilder.AlignmentType alignmentOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.