public interface AdmMoveFaceBuilder
AdmMoveFace
builder
FeatureCollection.createAdmMoveFaceBuilder(nxopen.features.AdmMoveFace)
Property | Value |
---|---|
FaceToMove.CoaxialEnabled | 0 |
FaceToMove.CoplanarAxesEnabled | 0 |
FaceToMove.CoplanarEnabled | 0 |
FaceToMove.EqualDiameterEnabled | 0 |
FaceToMove.OffsetEnabled | 0 |
FaceToMove.ParallelEnabled | 0 |
FaceToMove.PerpendicularEnabled | 0 |
FaceToMove.SymmetricEnabled | 0 |
FaceToMove.TangentEnabled | 0 |
FaceToMove.ThicknessChainEnabled | 0 |
FaceToMove.UseFaceBrowse | 1 |
HealOption | True |
Motion.DeltaEnum | ReferenceWcsWorkPart |
Motion.DeltaXc.Value | 0.0 |
Motion.DeltaYc.Value | 0.0 |
Motion.DeltaZc.Value | 0.0 |
Motion.Option | DistanceAngle |
StepOption.StepOption | None |
Modifier and Type | Interface and Description |
---|---|
static class |
AdmMoveFaceBuilder.MoveOptionType
Represents the move option.
|
Modifier and Type | Method and Description |
---|---|
nxopen.geometricutilities.FaceChangeOverflowBehavior |
faceChangeOverflowBehavior()
Returns the face change overflow behavior.
|
FaceRecognitionBuilder |
faceToMove()
Returns the face to move.
|
boolean |
healOption()
Returns the heal option.
|
ModlMotion |
motion()
Returns the motion.
|
AdmMoveFaceBuilder.MoveOptionType |
moveOption()
Returns the move option.
|
boolean |
pasteOption()
Returns the paste option.
|
void |
setHealOption(boolean healOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
void |
setMoveOption(AdmMoveFaceBuilder.MoveOptionType moveOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
void |
setPasteOption(boolean pasteOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
StepOptionBehavior |
stepOption()
Returns the step option behavior.
|
FaceRecognitionBuilder faceToMove() throws NXException, RemoteException
FaceRecognitionBuilder
for details.
NXException
RemoteException
ModlMotion motion() throws NXException, RemoteException
ModlMotion
for details.
NXException
RemoteException
nxopen.geometricutilities.FaceChangeOverflowBehavior faceChangeOverflowBehavior() throws NXException, RemoteException
nxopen.geometricutilities.FaceChangeOverflowBehavior
for details.
NXException
RemoteException
StepOptionBehavior stepOption() throws NXException, RemoteException
StepOptionBehavior
for details.
NXException
RemoteException
AdmMoveFaceBuilder.MoveOptionType moveOption() throws NXException, RemoteException
NXException
RemoteException
void setMoveOption(AdmMoveFaceBuilder.MoveOptionType moveOption) throws NXException, RemoteException
moveOption
- NXException
RemoteException
boolean pasteOption() throws NXException, RemoteException
NXException
RemoteException
void setPasteOption(boolean pasteOption) throws NXException, RemoteException
pasteOption
- NXException
RemoteException
boolean healOption() throws NXException, RemoteException
NXException
RemoteException
void setHealOption(boolean healOption) throws NXException, RemoteException
healOption
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.