public static class ViewPlacementBuilder.Method extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HORIZONTAL
Align the view horizontally to another view
|
static int |
_INFER
Infer the view position
|
static int |
_MAX
Should be the last enum in the list
|
static int |
_OVERLAY
Align the view on top of another view
|
static int |
_PERPENDICULAR_TO_HINGE_LINE
Align the view along the hinge line
|
static int |
_PERPENDICULAR_TO_LINE
Align the view along some line to another view
|
static int |
_VERTICAL
Align the view vertically to another view
|
static ViewPlacementBuilder.Method |
HORIZONTAL
Align the view horizontally to another view
|
static ViewPlacementBuilder.Method |
INFER
Infer the view position
|
static ViewPlacementBuilder.Method |
MAX
Should be the last enum in the list
|
static ViewPlacementBuilder.Method |
OVERLAY
Align the view on top of another view
|
static ViewPlacementBuilder.Method |
PERPENDICULAR_TO_HINGE_LINE
Align the view along the hinge line
|
static ViewPlacementBuilder.Method |
PERPENDICULAR_TO_LINE
Align the view along some line to another view
|
static ViewPlacementBuilder.Method |
VERTICAL
Align the view vertically to another view
|
Modifier and Type | Method and Description |
---|---|
static ViewPlacementBuilder.Method |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ViewPlacementBuilder.Method |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ViewPlacementBuilder.Method[] |
values()
Returns an array that contains the values for this enum.
|
public static final ViewPlacementBuilder.Method INFER
public static final ViewPlacementBuilder.Method HORIZONTAL
public static final ViewPlacementBuilder.Method VERTICAL
public static final ViewPlacementBuilder.Method PERPENDICULAR_TO_LINE
public static final ViewPlacementBuilder.Method OVERLAY
public static final ViewPlacementBuilder.Method PERPENDICULAR_TO_HINGE_LINE
public static final ViewPlacementBuilder.Method MAX
public static final int _INFER
public static final int _HORIZONTAL
public static final int _VERTICAL
public static final int _PERPENDICULAR_TO_LINE
public static final int _OVERLAY
public static final int _PERPENDICULAR_TO_HINGE_LINE
public static final int _MAX
public static ViewPlacementBuilder.Method valueOf(int value)
public static ViewPlacementBuilder.Method valueOf(String name)
public static ViewPlacementBuilder.Method[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.