Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static ViewPlacementBuilder.Method |
ViewPlacementBuilder.Method.HORIZONTAL
Align the view horizontally to another view
|
static ViewPlacementBuilder.Method |
ViewPlacementBuilder.Method.INFER
Infer the view position
|
static ViewPlacementBuilder.Method |
ViewPlacementBuilder.Method.MAX
Should be the last enum in the list
|
static ViewPlacementBuilder.Method |
ViewPlacementBuilder.Method.OVERLAY
Align the view on top of another view
|
static ViewPlacementBuilder.Method |
ViewPlacementBuilder.Method.PERPENDICULAR_TO_HINGE_LINE
Align the view along the hinge line
|
static ViewPlacementBuilder.Method |
ViewPlacementBuilder.Method.PERPENDICULAR_TO_LINE
Align the view along some line to another view
|
static ViewPlacementBuilder.Method |
ViewPlacementBuilder.Method.VERTICAL
Align the view vertically to another view
|
Modifier and Type | Method and Description |
---|---|
ViewPlacementBuilder.Method |
ViewPlacementBuilder.alignmentMethod()
Returns the alignment method
License requirements: None. |
static ViewPlacementBuilder.Method |
ViewPlacementBuilder.Method.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ViewPlacementBuilder.Method |
ViewPlacementBuilder.Method.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ViewPlacementBuilder.Method[] |
ViewPlacementBuilder.Method.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ViewPlacementBuilder.setAlignmentMethod(ViewPlacementBuilder.Method alignmentMethod)
License requirements: drafting ("DRAFTING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.