Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for display.
|
Modifier and Type | Field and Description |
---|---|
static Background.Type |
Background.Type.GRADUATED
two color background, which varies between them
|
static Background.Type |
Background.Type.HEMI_DOME
an 3D HDR image displayed in the background
|
static Background.Type |
Background.Type.IMAGE
an image file displayed in the background
|
static Background.Type |
Background.Type.PLAIN
single color background
|
Modifier and Type | Method and Description |
---|---|
Background.Type |
Background.backgroundType()
Returns the background type
License requirements: None. |
static Background.Type |
Background.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Background.Type |
Background.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Background.Type[] |
Background.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Background.setBackgroundType(Background.Type backgroundType)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.