public static class Background.Type extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_GRADUATED
two color background, which varies between them
|
static int |
_HEMI_DOME
an 3D HDR image displayed in the background
|
static int |
_IMAGE
an image file displayed in the background
|
static int |
_PLAIN
single color background
|
static Background.Type |
GRADUATED
two color background, which varies between them
|
static Background.Type |
HEMI_DOME
an 3D HDR image displayed in the background
|
static Background.Type |
IMAGE
an image file displayed in the background
|
static Background.Type |
PLAIN
single color background
|
Modifier and Type | Method and Description |
---|---|
static Background.Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Background.Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Background.Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final Background.Type PLAIN
public static final Background.Type GRADUATED
public static final Background.Type IMAGE
public static final Background.Type HEMI_DOME
public static final int _PLAIN
public static final int _GRADUATED
public static final int _IMAGE
public static final int _HEMI_DOME
public static Background.Type valueOf(int value)
public static Background.Type valueOf(String name)
public static Background.Type[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.