Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static UncutRegionsBuilder.ResultsType |
UncutRegionsBuilder.ResultsType.BOTH_SIDES
Find uncut regions on both sides of curve
|
static UncutRegionsBuilder.ResultsType |
UncutRegionsBuilder.ResultsType.ONE_SIDE
Find uncut regions on one side only
|
Modifier and Type | Method and Description |
---|---|
UncutRegionsBuilder.ResultsType |
UncutRegionsBuilder.results()
Returns the side of the curve to show the results.
|
static UncutRegionsBuilder.ResultsType |
UncutRegionsBuilder.ResultsType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static UncutRegionsBuilder.ResultsType |
UncutRegionsBuilder.ResultsType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static UncutRegionsBuilder.ResultsType[] |
UncutRegionsBuilder.ResultsType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
UncutRegionsBuilder.setResults(UncutRegionsBuilder.ResultsType results)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.