Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static TrimLineDevelopmentBuilder.Surface |
TrimLineDevelopmentBuilder.Surface.INNER
Onestep solver will offset inner surface and enlarge it
|
static TrimLineDevelopmentBuilder.Surface |
TrimLineDevelopmentBuilder.Surface.MIDDLE
Onestep solver will not offset middle surface
|
static TrimLineDevelopmentBuilder.Surface |
TrimLineDevelopmentBuilder.Surface.OUTER
Onestep solver will offset outer surface and shrink it
|
Modifier and Type | Method and Description |
---|---|
TrimLineDevelopmentBuilder.Surface |
TrimLineDevelopmentBuilder.surfaceType()
Returns the surface type used to determine offset direction.
|
static TrimLineDevelopmentBuilder.Surface |
TrimLineDevelopmentBuilder.Surface.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimLineDevelopmentBuilder.Surface |
TrimLineDevelopmentBuilder.Surface.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimLineDevelopmentBuilder.Surface[] |
TrimLineDevelopmentBuilder.Surface.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimLineDevelopmentBuilder.setSurfaceType(TrimLineDevelopmentBuilder.Surface surfaceType)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.