Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static TrimLineDevelopmentBuilder.MaterialTypeName |
TrimLineDevelopmentBuilder.MaterialTypeName.ALUMINUM
Aluminum
|
static TrimLineDevelopmentBuilder.MaterialTypeName |
TrimLineDevelopmentBuilder.MaterialTypeName.STEEL
Steel
|
Modifier and Type | Method and Description |
---|---|
TrimLineDevelopmentBuilder.MaterialTypeName |
TrimLineDevelopmentBuilder.materialType()
Returns the material type - steel or aluminum
License requirements: None. |
static TrimLineDevelopmentBuilder.MaterialTypeName |
TrimLineDevelopmentBuilder.MaterialTypeName.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimLineDevelopmentBuilder.MaterialTypeName |
TrimLineDevelopmentBuilder.MaterialTypeName.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimLineDevelopmentBuilder.MaterialTypeName[] |
TrimLineDevelopmentBuilder.MaterialTypeName.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimLineDevelopmentBuilder.setMaterialType(TrimLineDevelopmentBuilder.MaterialTypeName materialType)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.