Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static ThroatParentBuilder.TypeOption |
ThroatParentBuilder.TypeOption.RESTRIKE
Throat is built for a restrike operation.
|
static ThroatParentBuilder.TypeOption |
ThroatParentBuilder.TypeOption.WIPE
Throat is built for a wipe operation.
|
Modifier and Type | Method and Description |
---|---|
ThroatParentBuilder.TypeOption |
ThroatParentBuilder.type()
Returns the type of throat sections.
|
static ThroatParentBuilder.TypeOption |
ThroatParentBuilder.TypeOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThroatParentBuilder.TypeOption |
ThroatParentBuilder.TypeOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThroatParentBuilder.TypeOption[] |
ThroatParentBuilder.TypeOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ThroatParentBuilder.setType(ThroatParentBuilder.TypeOption type)
Sets the type of throat sections.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.