Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static ThroatChildBuilder.TypeOption |
ThroatChildBuilder.TypeOption.RESTRIKE
Throat section is built for a restrike operation.
|
static ThroatChildBuilder.TypeOption |
ThroatChildBuilder.TypeOption.WIPE
Throat section is built for a wipe operation.
|
Modifier and Type | Method and Description |
---|---|
static ThroatChildBuilder.TypeOption |
ThroatChildBuilder.TypeOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ThroatChildBuilder.TypeOption |
ThroatChildBuilder.TypeOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ThroatChildBuilder.TypeOption[] |
ThroatChildBuilder.TypeOption.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.