Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static SteelInsertSegmentParentBuilder.ExtensionTypeOption |
SteelInsertSegmentParentBuilder.ExtensionTypeOption.CONSTANT
constant
|
static SteelInsertSegmentParentBuilder.ExtensionTypeOption |
SteelInsertSegmentParentBuilder.ExtensionTypeOption.LAW
law
|
static SteelInsertSegmentParentBuilder.ExtensionTypeOption |
SteelInsertSegmentParentBuilder.ExtensionTypeOption.MAXDIST_PLUS_CONST
maximum distance + constant
|
Modifier and Type | Method and Description |
---|---|
SteelInsertSegmentParentBuilder.ExtensionTypeOption |
SteelInsertSegmentParentBuilder.extensionType()
Returns the extension type
License requirements: ug_die_design ("Die Design") . |
static SteelInsertSegmentParentBuilder.ExtensionTypeOption |
SteelInsertSegmentParentBuilder.ExtensionTypeOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SteelInsertSegmentParentBuilder.ExtensionTypeOption |
SteelInsertSegmentParentBuilder.ExtensionTypeOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SteelInsertSegmentParentBuilder.ExtensionTypeOption[] |
SteelInsertSegmentParentBuilder.ExtensionTypeOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SteelInsertSegmentParentBuilder.setExtensionType(SteelInsertSegmentParentBuilder.ExtensionTypeOption extensionType)
Sets the extension type
License requirements: ug_die_design ("Die Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.