Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static SpringbackCompensationBuilder.ResultSheetType |
SpringbackCompensationBuilder.ResultSheetType.COMPENSATED
Compensated sheet body.
|
static SpringbackCompensationBuilder.ResultSheetType |
SpringbackCompensationBuilder.ResultSheetType.SPRUNG
Sprung sheet body.
|
Modifier and Type | Method and Description |
---|---|
SpringbackCompensationBuilder.ResultSheetType |
SpringbackCompensationBuilder.resultType()
Returns the type of output to generate.
|
static SpringbackCompensationBuilder.ResultSheetType |
SpringbackCompensationBuilder.ResultSheetType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpringbackCompensationBuilder.ResultSheetType |
SpringbackCompensationBuilder.ResultSheetType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpringbackCompensationBuilder.ResultSheetType[] |
SpringbackCompensationBuilder.ResultSheetType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SpringbackCompensationBuilder.setResultType(SpringbackCompensationBuilder.ResultSheetType resultType)
License requirements: die_engineering ("DIE ENGINEERING") OR nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.