Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static PierceTaskBuilder.PrecisionTypes |
PierceTaskBuilder.PrecisionTypes.CRITICAL
Critical hole
|
static PierceTaskBuilder.PrecisionTypes |
PierceTaskBuilder.PrecisionTypes.GAGE
Gage hole
|
static PierceTaskBuilder.PrecisionTypes |
PierceTaskBuilder.PrecisionTypes.STANDARD
Standard hole
|
Modifier and Type | Method and Description |
---|---|
PierceTaskBuilder.PrecisionTypes |
PierceTaskBuilder.precisionType()
Returns the precision type of the pierce task
License requirements: die_engineering ("DIE ENGINEERING") . |
static PierceTaskBuilder.PrecisionTypes |
PierceTaskBuilder.PrecisionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PierceTaskBuilder.PrecisionTypes |
PierceTaskBuilder.PrecisionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PierceTaskBuilder.PrecisionTypes[] |
PierceTaskBuilder.PrecisionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PierceTaskBuilder.setPrecisionType(PierceTaskBuilder.PrecisionTypes precisionType)
Sets the precision type of the pierce task
License requirements: die_engineering ("DIE ENGINEERING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.