Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static PierceTaskBuilder.CamTypes |
PierceTaskBuilder.CamTypes.AERIAL
Aerial Cam
|
static PierceTaskBuilder.CamTypes |
PierceTaskBuilder.CamTypes.BASE_MOUNTED
Base Mounted Cam
|
static PierceTaskBuilder.CamTypes |
PierceTaskBuilder.CamTypes.DIRECT
Direct
|
Modifier and Type | Method and Description |
---|---|
PierceTaskBuilder.CamTypes |
PierceTaskBuilder.camType()
Returns the cam type of the pierce task
License requirements: die_engineering ("DIE ENGINEERING") . |
static PierceTaskBuilder.CamTypes |
PierceTaskBuilder.CamTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PierceTaskBuilder.CamTypes |
PierceTaskBuilder.CamTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PierceTaskBuilder.CamTypes[] |
PierceTaskBuilder.CamTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PierceTaskBuilder.setCamType(PierceTaskBuilder.CamTypes camType)
Sets the cam type of the pierce task
License requirements: die_engineering ("DIE ENGINEERING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.