Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Method and Description |
---|---|
PierceItemBuilder |
PierceItemBuilderList.findItem(int index)
Returns the object at the input index.
|
PierceItemBuilder[] |
PierceItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
PierceItemBuilder |
PierceTaskBuilder.newPierceHole(PierceItemBuilder.HoleShapeType holeShape)
Creates a new pierce hole item in the set
License requirements: die_engineering ("DIE ENGINEERING") . |
Modifier and Type | Method and Description |
---|---|
void |
PierceItemBuilderList.append(PierceItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
PierceItemBuilderList.append(PierceItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PierceItemBuilderList.erase(PierceItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
PierceItemBuilderList.erase(PierceItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PierceItemBuilderList.findIndex(PierceItemBuilder obj)
Finds the index where the input object appears.
|
void |
PierceItemBuilderList.insert(int location,
PierceItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
PierceItemBuilderList.setContents(PierceItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
PierceItemBuilderList.swap(PierceItemBuilder object1,
PierceItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.