Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static PierceItemBuilder.SizingMethodOption |
PierceItemBuilder.SizingMethodOption.AUTO
Will calculate size at creation and during update
|
static PierceItemBuilder.SizingMethodOption |
PierceItemBuilder.SizingMethodOption.MANUAL
Will use size specified
|
Modifier and Type | Method and Description |
---|---|
PierceItemBuilder.SizingMethodOption |
PierceItemBuilder.sizingMethod()
Returns the sizing method
License requirements: None. |
static PierceItemBuilder.SizingMethodOption |
PierceItemBuilder.SizingMethodOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PierceItemBuilder.SizingMethodOption |
PierceItemBuilder.SizingMethodOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PierceItemBuilder.SizingMethodOption[] |
PierceItemBuilder.SizingMethodOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PierceItemBuilder.setSizingMethod(PierceItemBuilder.SizingMethodOption sizingMethod)
License requirements: die_engineering ("DIE ENGINEERING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.