Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static MachineReliefBuilder.MainProfileTypes |
MachineReliefBuilder.MainProfileTypes.EXTERIOR
Profile is for the exterior surface of the main wall.
|
static MachineReliefBuilder.MainProfileTypes |
MachineReliefBuilder.MainProfileTypes.INTERIOR
Profile is for the interior surface of the main wall.
|
Modifier and Type | Method and Description |
---|---|
MachineReliefBuilder.MainProfileTypes |
MachineReliefBuilder.mainProfileType()
Returns the value specifying the main profile for the Thicken operation.
|
static MachineReliefBuilder.MainProfileTypes |
MachineReliefBuilder.MainProfileTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MachineReliefBuilder.MainProfileTypes |
MachineReliefBuilder.MainProfileTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MachineReliefBuilder.MainProfileTypes[] |
MachineReliefBuilder.MainProfileTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MachineReliefBuilder.setMainProfileType(MachineReliefBuilder.MainProfileTypes mainProfileType)
License requirements: ug_die_design ("Die Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.