Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static HandlingCoreBuilder.Types |
HandlingCoreBuilder.Types.AT_LOCATION
Location specified by the user.
|
static HandlingCoreBuilder.Types |
HandlingCoreBuilder.Types.FROM_BASE
Location is an offset from the base.
|
static HandlingCoreBuilder.Types |
HandlingCoreBuilder.Types.MAP_FROM_BASE
Locate by finding the minimum distance to the main profile of the target and then project and offset from the base.
|
Modifier and Type | Method and Description |
---|---|
HandlingCoreBuilder.Types |
HandlingCoreBuilder.type()
Returns the indicator defining how the handling core is located in space.
|
static HandlingCoreBuilder.Types |
HandlingCoreBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HandlingCoreBuilder.Types |
HandlingCoreBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HandlingCoreBuilder.Types[] |
HandlingCoreBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HandlingCoreBuilder.setType(HandlingCoreBuilder.Types type)
License requirements: ug_die_design ("Die Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.