Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static FillAreaBuilder.UpperLimitTypes |
FillAreaBuilder.UpperLimitTypes.PLANE
Upper limit is defined by a plane.
|
static FillAreaBuilder.UpperLimitTypes |
FillAreaBuilder.UpperLimitTypes.SHEET
Upper limit is defined by a sheet body.
|
Modifier and Type | Method and Description |
---|---|
FillAreaBuilder.UpperLimitTypes |
FillAreaBuilder.upperLimitType()
Returns the value that determines whether the upper limit is defined by a sheet or plane.
|
static FillAreaBuilder.UpperLimitTypes |
FillAreaBuilder.UpperLimitTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FillAreaBuilder.UpperLimitTypes |
FillAreaBuilder.UpperLimitTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FillAreaBuilder.UpperLimitTypes[] |
FillAreaBuilder.UpperLimitTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FillAreaBuilder.setUpperLimitType(FillAreaBuilder.UpperLimitTypes upperLimitType)
License requirements: ug_die_design ("Die Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.