Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DrawBeadSegmentBuilder.MaleBeadWidthTypes |
DrawBeadSegmentBuilder.MaleBeadWidthTypes.CONSTANT
The male bead width is specified by a constant value.
|
static DrawBeadSegmentBuilder.MaleBeadWidthTypes |
DrawBeadSegmentBuilder.MaleBeadWidthTypes.DERIVED
The male bead width is derived from the width specified for the female.
|
Modifier and Type | Method and Description |
---|---|
DrawBeadSegmentBuilder.MaleBeadWidthTypes |
DrawBeadSegmentBuilder.maleBeadWidthType()
Returns the male bead width type.
|
static DrawBeadSegmentBuilder.MaleBeadWidthTypes |
DrawBeadSegmentBuilder.MaleBeadWidthTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadSegmentBuilder.MaleBeadWidthTypes |
DrawBeadSegmentBuilder.MaleBeadWidthTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadSegmentBuilder.MaleBeadWidthTypes[] |
DrawBeadSegmentBuilder.MaleBeadWidthTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawBeadSegmentBuilder.setMaleBeadWidthType(DrawBeadSegmentBuilder.MaleBeadWidthTypes maleBeadWidthType)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.