Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DrawBeadBuilder.TransitionDefinitionTypes |
DrawBeadBuilder.TransitionDefinitionTypes.AUTOMATIC
Shorten the bead segment that has the lowest height.
|
static DrawBeadBuilder.TransitionDefinitionTypes |
DrawBeadBuilder.TransitionDefinitionTypes.MANUAL
User specified start and end segments so transition areas are fully defined.
|
Modifier and Type | Method and Description |
---|---|
DrawBeadBuilder.TransitionDefinitionTypes |
DrawBeadBuilder.transitionDefinition()
Returns the method used to build the transition between segments.
|
static DrawBeadBuilder.TransitionDefinitionTypes |
DrawBeadBuilder.TransitionDefinitionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.TransitionDefinitionTypes |
DrawBeadBuilder.TransitionDefinitionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.TransitionDefinitionTypes[] |
DrawBeadBuilder.TransitionDefinitionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawBeadBuilder.setTransitionDefinition(DrawBeadBuilder.TransitionDefinitionTypes transitionDefinition)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.