Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DrawBeadBuilder.OrientSectionToDrawTypes |
DrawBeadBuilder.OrientSectionToDrawTypes.DRAW_DIRECTION
Orient height parameter to the draw direction.
|
static DrawBeadBuilder.OrientSectionToDrawTypes |
DrawBeadBuilder.OrientSectionToDrawTypes.SHEET_METAL_NORMAL
Orient height parameter to the sheet metal normal at the section location.
|
Modifier and Type | Method and Description |
---|---|
DrawBeadBuilder.OrientSectionToDrawTypes |
DrawBeadBuilder.orientSectionToDraw()
Returns the method used to orient the section dimensions.
|
static DrawBeadBuilder.OrientSectionToDrawTypes |
DrawBeadBuilder.OrientSectionToDrawTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.OrientSectionToDrawTypes |
DrawBeadBuilder.OrientSectionToDrawTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.OrientSectionToDrawTypes[] |
DrawBeadBuilder.OrientSectionToDrawTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawBeadBuilder.setOrientSectionToDraw(DrawBeadBuilder.OrientSectionToDrawTypes orientSectionToDraw)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.