Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Method and Description |
---|---|
DieLimitsBuilder |
DieCollection.createDieLimits()
Creates a
DieLimitsBuilder . |
DieLimitsBuilder |
DieLimitsBuilderList.findItem(int index)
Returns the object at the input index.
|
DieLimitsBuilder[] |
DieLimitsBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
DieLimitsBuilder |
TrimLineDevelopmentBuilder.limits()
Returns the limits to control the span of the addendum
License requirements: None. |
DieLimitsBuilder |
AddSurfBuilder.limits()
Returns the limits to control the span of the addendum
License requirements: None. |
DieLimitsBuilder |
AddendumSectionBuilder.limits()
Returns the limits to control the span of the preview surface
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DieLimitsBuilderList.append(DieLimitsBuilder object)
Appends an object to the list
License requirements: None. |
void |
DieLimitsBuilderList.append(DieLimitsBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
DieLimitsBuilderList.erase(DieLimitsBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
DieLimitsBuilderList.erase(DieLimitsBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
DieLimitsBuilderList.findIndex(DieLimitsBuilder obj)
Finds the index where the input object appears.
|
void |
DieLimitsBuilderList.insert(int location,
DieLimitsBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
DieLimitsBuilderList.setContents(DieLimitsBuilder[] objects)
Sets the contents of the entire list.
|
void |
DieLimitsBuilderList.swap(DieLimitsBuilder object1,
DieLimitsBuilder object2)
Exchanges the position of two objects inside the list.
|
Modifier and Type | Method and Description |
---|---|
DieLimitsBuilder |
PatchOpeningsBuilder.limits()
Returns the limits to control the span of the patch
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
DieLimitsBuilder |
WeldJointBuilder.getJointLimits(Curve curve)
Get the limits of an individual joint.
|
DieLimitsBuilder |
WeldJointBuilder.limits()
Returns the limits of the joint curve span.
|
DieLimitsBuilder |
JointItemBuilder.limits()
Returns the limits of the joint curve span.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldJointBuilder.copyLimits(DieLimitsBuilder limits)
Copy input limits to builder limits
License requirements: None. |
void |
WeldJointBuilder.updateJointAfterLimitsChange(DieLimitsBuilder limits)
Updates the joint curve after the limits change.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.