Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Method and Description |
---|---|
DieDirectionBuilder |
MachineReliefBuilder.camDirection()
Returns the direction of the cam for trimming.
|
DieDirectionBuilder |
DieShoeBuilder.centerlineSlotDirection()
Returns the centerline slot direction
License requirements: None. |
DieDirectionBuilder |
FingerClearanceNotchBuilder.clearanceDirection()
Returns the direction (pointing away from the solid) in which to clear material from the target solid.
|
DieDirectionBuilder |
ClearanceBuilder.clearanceDirection()
Returns the direction to use when extruding to create the clearance areas.
|
DieDirectionBuilder |
DieCollection.createDieDirection(nxopen.features.Feature feature)
Creates a
DieDirectionBuilder . |
DieDirectionBuilder |
DrawBeadBuilder.drawDirection()
Returns the draw direction.
|
DieDirectionBuilder |
ClampingSlotBuilder.locationOffsetDirection()
Returns the direction to offset the clampslot locations if needed
License requirements: None. |
DieDirectionBuilder |
HeelpostBuilder.offsetDirection()
Returns the direction to apply to the location to determine the center of the heelpost
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.