Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Method and Description |
---|---|
DieBooleanBuilder |
DieCollection.createDieBoolean()
Creates a
DieBooleanBuilder . |
DieBooleanBuilder |
DieBooleanBuilderList.findItem(int index)
Returns the object at the input index.
|
DieBooleanBuilder[] |
DieBooleanBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DieBooleanBuilderList.append(DieBooleanBuilder object)
Appends an object to the list
License requirements: None. |
void |
DieBooleanBuilderList.append(DieBooleanBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
DieBooleanBuilderList.erase(DieBooleanBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
DieBooleanBuilderList.erase(DieBooleanBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
DieBooleanBuilderList.findIndex(DieBooleanBuilder obj)
Finds the index where the input object appears.
|
void |
DieBooleanBuilderList.insert(int location,
DieBooleanBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
DieBooleanBuilderList.setContents(DieBooleanBuilder[] objects)
Sets the contents of the entire list.
|
void |
DieBooleanBuilderList.swap(DieBooleanBuilder object1,
DieBooleanBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.