Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DieBooleanBuilder.BooleanType |
DieBooleanBuilder.BooleanType.INTERSECT
Intersect the solids with the application solid.
|
static DieBooleanBuilder.BooleanType |
DieBooleanBuilder.BooleanType.SUBTRACT
Subtract the solids from the application solid.
|
static DieBooleanBuilder.BooleanType |
DieBooleanBuilder.BooleanType.UNITE
Unite the solids to the application solid.
|
Modifier and Type | Method and Description |
---|---|
DieBooleanBuilder.BooleanType |
DieBooleanBuilder.booleanOptions()
Returns the boolean option to apply to the list of selected solids
License requirements: None. |
static DieBooleanBuilder.BooleanType |
DieBooleanBuilder.BooleanType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieBooleanBuilder.BooleanType |
DieBooleanBuilder.BooleanType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieBooleanBuilder.BooleanType[] |
DieBooleanBuilder.BooleanType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieBooleanBuilder.setBooleanOptions(DieBooleanBuilder.BooleanType booleanOptions)
License requirements: ug_die_design ("Die Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.