Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static CompensateRoughDataBuilder.Types |
CompensateRoughDataBuilder.Types.CURVE
Curves being compensated.
|
static CompensateRoughDataBuilder.Types |
CompensateRoughDataBuilder.Types.SHEET_BODY
Sheet bodies being compensated.
|
Modifier and Type | Method and Description |
---|---|
CompensateRoughDataBuilder.Types |
CompensateRoughDataBuilder.type()
Returns the type of input data being supplied.
|
static CompensateRoughDataBuilder.Types |
CompensateRoughDataBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CompensateRoughDataBuilder.Types |
CompensateRoughDataBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CompensateRoughDataBuilder.Types[] |
CompensateRoughDataBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CompensateRoughDataBuilder.setType(CompensateRoughDataBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.