Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static AddendumSectionBuilder.SurfaceBuildType |
AddendumSectionBuilder.SurfaceBuildType.CHANNEL_TUNNEL_CAP
Create channel tunnel cap surface.
|
static AddendumSectionBuilder.SurfaceBuildType |
AddendumSectionBuilder.SurfaceBuildType.CURVE_MESH
Create curve mesh surface.
|
static AddendumSectionBuilder.SurfaceBuildType |
AddendumSectionBuilder.SurfaceBuildType.DISK_FACE_BLEND
Create disc blend surface.
|
static AddendumSectionBuilder.SurfaceBuildType |
AddendumSectionBuilder.SurfaceBuildType.MULTIPLE_FACE_BLEND
Create multiple face blend surface.
|
static AddendumSectionBuilder.SurfaceBuildType |
AddendumSectionBuilder.SurfaceBuildType.NO_SURFACE
Do not create a surface.
|
static AddendumSectionBuilder.SurfaceBuildType |
AddendumSectionBuilder.SurfaceBuildType.SECTIONAL
Create sectional sweep surface.
|
static AddendumSectionBuilder.SurfaceBuildType |
AddendumSectionBuilder.SurfaceBuildType.SPHERE_FACE_BLEND
Create spherical blend surface.
|
static AddendumSectionBuilder.SurfaceBuildType |
AddendumSectionBuilder.SurfaceBuildType.WALLS_ONLY
Create walls only surface.
|
Modifier and Type | Method and Description |
---|---|
AddendumSectionBuilder.SurfaceBuildType |
AddendumSectionBuilder.surfaceBuildMethod()
Returns the addendum surface build method.
|
static AddendumSectionBuilder.SurfaceBuildType |
AddendumSectionBuilder.SurfaceBuildType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AddendumSectionBuilder.SurfaceBuildType |
AddendumSectionBuilder.SurfaceBuildType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AddendumSectionBuilder.SurfaceBuildType[] |
AddendumSectionBuilder.SurfaceBuildType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AddendumSectionBuilder.setSurfaceBuildMethod(AddendumSectionBuilder.SurfaceBuildType surfaceBuildMethod)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.