Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static AddSurfBuilder.Methods |
AddSurfBuilder.Methods.CHANNEL_TUNNEL_CAP
To close an end cap.
|
static AddSurfBuilder.Methods |
AddSurfBuilder.Methods.CURVE_MESH
Modeling curve mesh.
|
static AddSurfBuilder.Methods |
AddSurfBuilder.Methods.DISK_FACE_BLEND
Disk type face blend.
|
static AddSurfBuilder.Methods |
AddSurfBuilder.Methods.MULTI_FACE_BLEND
Face blend between sets of walls.
|
static AddSurfBuilder.Methods |
AddSurfBuilder.Methods.SECTIONAL
Sweep section around tangency curve.
|
static AddSurfBuilder.Methods |
AddSurfBuilder.Methods.SPHERE_FACE_BLEND
Spherical type face blend.
|
static AddSurfBuilder.Methods |
AddSurfBuilder.Methods.WALLS_ONLY
Produces just the walls, no blend.
|
Modifier and Type | Method and Description |
---|---|
AddSurfBuilder.Methods |
AddSurfBuilder.method()
Returns the addendum surface output method.
|
static AddSurfBuilder.Methods |
AddSurfBuilder.Methods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AddSurfBuilder.Methods |
AddSurfBuilder.Methods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AddSurfBuilder.Methods[] |
AddSurfBuilder.Methods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AddSurfBuilder.setMethod(AddSurfBuilder.Methods type)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.