Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Sketch.AssocType |
Sketch.AssocType.ANCHOR_POINT
The anchor of a conic
|
static Sketch.AssocType |
Sketch.AssocType.ARC_CENTER
Center of an arc, circle, or ellipse
|
Sketch.AssocType |
Sketch.DimensionGeometry.assocType |
static Sketch.AssocType |
Sketch.AssocType.CURVE_POINT
A point on a spline
|
static Sketch.AssocType |
Sketch.AssocType.END_POINT
End point.
|
static Sketch.AssocType |
Sketch.AssocType.MIDPOINT
The midpoint of a curve
|
static Sketch.AssocType |
Sketch.AssocType.NONE
Use the entire geometric item, as opposed to a point
|
static Sketch.AssocType |
Sketch.AssocType.START_POINT
Start point.
|
static Sketch.AssocType |
Sketch.AssocType.TANGENCY
Create the dimension tangent to the geometric item
|
Modifier and Type | Method and Description |
---|---|
static Sketch.AssocType |
Sketch.AssocType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.AssocType |
Sketch.AssocType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.AssocType[] |
Sketch.AssocType.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
DimensionGeometry(NXObject geometryInitial,
Sketch.AssocType assocTypeInitial,
int assocValueInitial,
Point3d helpPointInitial,
NXObject viewInitial)
Constructor for the DimensionGeometry object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.