public static class Sketch.DimensionGeometry extends Object implements Serializable
Examples: 1. To specify the start point of line1 Geometry = line1 AssocType = StartPoint AssocValue = 0
Modifier and Type | Field and Description |
---|---|
Sketch.AssocType |
assocType |
int |
assocValue
See table for meaning.
|
NXObject |
geometry |
Point3d |
helpPoint
help point
|
NXObject |
view
The view the geometry is dependent on, if any
|
Constructor and Description |
---|
DimensionGeometry() |
DimensionGeometry(NXObject geometryInitial,
Sketch.AssocType assocTypeInitial,
int assocValueInitial,
Point3d helpPointInitial,
NXObject viewInitial)
Constructor for the DimensionGeometry object.
|
public NXObject geometry
public Sketch.AssocType assocType
public int assocValue
The AssocValue has the following meanings: AssocType AssocValue meaning ---------- ------------------- Tangency parameter percentage (0 - 100) (used to find approximate tangent point) CurvePoint the index number of the defining point of the spline(starting from 1) all else not used
public Point3d helpPoint
public NXObject view
public DimensionGeometry()
public DimensionGeometry(NXObject geometryInitial, Sketch.AssocType assocTypeInitial, int assocValueInitial, Point3d helpPointInitial, NXObject viewInitial)
geometryInitial
- assocTypeInitial
- assocValueInitial
- See table for meaning.
The AssocValue has the following meanings: AssocType AssocValue meaning ---------- ------------------- Tangency parameter percentage (0 - 100) (used to find approximate tangent point) CurvePoint the index number of the defining point of the spline(starting from 1) all else not used
helpPointInitial
- help pointviewInitial
- The view the geometry is dependent on, if anyCopyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.