Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.uistyler |
PProvides classes and interfaces for User Interface (UI) Styler.
|
Modifier and Type | Method and Description |
---|---|
void |
Selection.addToSelectionList(SelectionHandle select,
NXObject[] objs,
boolean highlightFlag)
Deprecated.
Deprecated in NX8.0.0. Use
Selection.addToTaggedObjectsSelectionList(nxopen.SelectionHandle, nxopen.TaggedObject[], boolean) instead
|
void |
Selection.addToTaggedObjectsSelectionList(SelectionHandle select,
TaggedObject[] objs,
boolean highlightFlag)
Add objects to the selection list.
|
Selection.AskSelectionCursorPositionData |
Selection.askSelectionCursorPosition(SelectionHandle select)
Returns the view and absolute coordinates of the cursor position for the associated selection.
|
Selection.SelectionDescriptor |
Selection.askSelectionDescriptor(SelectionHandle select)
Returns the information in
Selection.SelectionDescriptor
describing the selection that was just performed. |
int |
Selection.askSelectionListCount(SelectionHandle select)
Returns the number of objects currently selected.
|
NXObject[] |
Selection.askSelectionObjectList(SelectionHandle select)
Deprecated.
Deprecated in NX8.0.0. Use
Selection.askSelectionTaggedObjectList(nxopen.SelectionHandle) instead
|
Selection.AskSelectionRectanglePositionData |
Selection.askSelectionRectanglePosition(SelectionHandle select)
Returns the absolute coordinates of the rectangle cursor positions.
|
TaggedObject[] |
Selection.askSelectionTaggedObjectList(SelectionHandle select)
Returns the number of tagged objects selected and a pointer to an array of
tags of the objects selected.
|
int |
Selection.FilterCallback.filterCallback(NXObject entity,
Selection.MaskTriple entityMask,
SelectionHandle selectHandle)
Deprecated.
Deprecated in NX8.0.0. Use
Selection#filterTaggedObjectCallback instead
|
int |
Selection.FilterTaggedObjectCallback.filterTaggedObjectCallback(TaggedObject entity,
Selection.MaskTriple entityMask,
SelectionHandle selectHandle)
It is an optional callback which the user can provide to perform
application specific filtering when selecting tagged objects.
|
boolean |
Selection.isObjectInSelectionList(SelectionHandle select,
TaggedObject object)
Inquires if object is selected.
|
void |
Selection.removeAllFromSelectionList(SelectionHandle select,
boolean unhighlight)
Removes all the objects from the selection list and optionally unhighlights them.
|
void |
Selection.removeFromSelectionList(SelectionHandle select,
NXObject[] objs,
boolean unhighlight)
Deprecated.
Deprecated in NX8.0.0. Use
Selection.removeTaggedObjectsFromSelectionList(nxopen.SelectionHandle, nxopen.TaggedObject[], boolean) instead
|
void |
Selection.removeTaggedObjectsFromSelectionList(SelectionHandle select,
TaggedObject[] objs,
boolean unhighlight)
Removes tagged objects from the selection list.
|
int |
Selection.SelectionCallback.selectionCallback(NXObject[] selectedObjects,
NXObject[] deselectedObjects,
SelectionHandle selectHandle)
Deprecated.
Deprecated in NX8.0.0. Use
Selection#taggedObjectSelectionCallback instead
|
void |
Selection.setSelectionCallbacks(SelectionHandle select,
Selection.FilterCallback filterproc,
Selection.SelectionCallback selcb)
Deprecated.
|
void |
Selection.setSelectionMask(SelectionHandle select,
Selection.SelectionAction action,
Selection.MaskTriple[] maskArray)
Sets the types of objects that are selectable.
|
void |
Selection.setSelectType(SelectionHandle select,
Selection.UistylerSelectionType type)
Sets the selection type.
|
void |
Selection.setTaggedObjectSelectionCallbacks(SelectionHandle select,
Selection.FilterTaggedObjectCallback filterproc,
Selection.TaggedObjectSelectionCallback selcb)
Specify selection filter callback for additional filtering of tagged objects based on
application specific criteria, and/or selection callback to perform
application specific processing for each selection gesture processed.
|
int |
Selection.TaggedObjectSelectionCallback.taggedObjectSelectionCallback(TaggedObject[] selectedObjects,
TaggedObject[] deselectedObjects,
SelectionHandle selectHandle)
It is an optional callback which the user can provide to customize his selection of tagged objects
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectionHandle |
DialogItem.getSelectionHandle()
Gets the selection handle for a given dialog item
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
StylerItem |
Dialog.getDialogItemUsingSelectionHandle(SelectionHandle select)
Gets the dialog item for a selection handle
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.