public static class Selection.UistylerSelectionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INACTIVE_SELECTION
sets selection inactive until
this function is called again
|
static int |
_RECTANGLE_POSITION
the position is returned if no object is selected with the
single select gesture
|
static int |
_ROBUST_SELECTION
reselect last
|
static int |
_SINGLE_DESELECTION
single deselect
|
static int |
_SINGLE_POSITION
the position is returned if no object is selected with the
single select gesture
|
static int |
_SINGLE_SELECTION
allows
single select
|
static Selection.UistylerSelectionType |
INACTIVE_SELECTION
sets selection inactive until
this function is called again
|
static Selection.UistylerSelectionType |
RECTANGLE_POSITION
the position is returned if no object is selected with the
single select gesture
|
static Selection.UistylerSelectionType |
ROBUST_SELECTION
reselect last
|
static Selection.UistylerSelectionType |
SINGLE_DESELECTION
single deselect
|
static Selection.UistylerSelectionType |
SINGLE_POSITION
the position is returned if no object is selected with the
single select gesture
|
static Selection.UistylerSelectionType |
SINGLE_SELECTION
allows
single select
|
Modifier and Type | Method and Description |
---|---|
static Selection.UistylerSelectionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Selection.UistylerSelectionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Selection.UistylerSelectionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final Selection.UistylerSelectionType INACTIVE_SELECTION
public static final Selection.UistylerSelectionType SINGLE_SELECTION
public static final Selection.UistylerSelectionType SINGLE_DESELECTION
public static final Selection.UistylerSelectionType ROBUST_SELECTION
public static final Selection.UistylerSelectionType SINGLE_POSITION
public static final Selection.UistylerSelectionType RECTANGLE_POSITION
public static final int _INACTIVE_SELECTION
public static final int _SINGLE_SELECTION
public static final int _SINGLE_DESELECTION
public static final int _ROBUST_SELECTION
public static final int _SINGLE_POSITION
public static final int _RECTANGLE_POSITION
public static Selection.UistylerSelectionType valueOf(int value)
public static Selection.UistylerSelectionType valueOf(String name)
public static Selection.UistylerSelectionType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.