Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
nxopen.visualreporting |
Provides classes and interfaces for Visual Reporting.
|
Modifier and Type | Method and Description |
---|---|
NXColor.Rgb |
NXColor.getRgb()
Gets the RGB values in the display part
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
Post.postviewSetColorbar(int postviewId,
Post.Colorbar colorbar,
boolean customOverwrite,
double[] rangeValue,
NXColor.Rgb[] rangeColors)
Set color bar options along with custom overwrite options in the input postview id.
|
Modifier and Type | Field and Description |
---|---|
NXColor.Rgb |
PartVisualizationEmphasis.ShellOptions.edgesRgb
the color of edges displayed for de-emphasized shaded
geometry when the See-Thru style is set to Shell.
|
NXColor.Rgb |
PartVisualizationEmphasis.OriginalColorShellOptions.edgesRgb
the color of edges displayed for de-emphasized shaded
geometry when the See-Thru style is set to Original Color
Shell.
|
NXColor.Rgb |
PartVisualizationEmphasis.LayersOptions.edgesRgb
the color of edges displayed for de-emphasized shaded
geometry when the See-Thru style is set to Layers.
|
NXColor.Rgb |
PartVisualizationEmphasis.ShellOptions.rgb
the color of de-emphasized shaded geometry when the
See-Thru style is set to Shell.
|
NXColor.Rgb |
PartVisualizationEmphasis.LayersOptions.rgb
the color of de-emphasized shaded geometry when the
See-Thru style is set to Layers.
|
Constructor and Description |
---|
LayersOptions(NXColor.Rgb rgbInitial,
PartVisualizationEmphasis.EdgesType edgesInitial,
NXColor.Rgb edgesRgbInitial,
int translucencyInitial)
Constructor for the LayersOptions object.
|
OriginalColorShellOptions(PartVisualizationEmphasis.EdgesType edgesInitial,
NXColor.Rgb edgesRgbInitial,
int translucencyInitial)
Constructor for the OriginalColorShellOptions object.
|
ShellOptions(NXColor.Rgb rgbInitial,
PartVisualizationEmphasis.EdgesType edgesInitial,
NXColor.Rgb edgesRgbInitial,
int translucencyInitial)
Constructor for the ShellOptions object.
|
Modifier and Type | Method and Description |
---|---|
NXColor.Rgb |
GroupLabel.color()
Returns the color of the
GroupLabel
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
GroupLabel.setColor(NXColor.Rgb color)
License requirements: nx_visual_reporting ("Visual Reporting") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.