Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static MovieSettingsBuilder.PlaybackSpeedChoices |
MovieSettingsBuilder.PlaybackSpeedChoices.AS_RECORDED
Specifies playback speed same as record speed
|
static MovieSettingsBuilder.PlaybackSpeedChoices |
MovieSettingsBuilder.PlaybackSpeedChoices.FAST
Specifies fast playback speed (twice record speed)
|
static MovieSettingsBuilder.PlaybackSpeedChoices |
MovieSettingsBuilder.PlaybackSpeedChoices.SLOW
Specifies slow playback speed (half of record speed)
|
static MovieSettingsBuilder.PlaybackSpeedChoices |
MovieSettingsBuilder.PlaybackSpeedChoices.VERY_FAST
Specifies very fast playback speed (four times record speed)
|
static MovieSettingsBuilder.PlaybackSpeedChoices |
MovieSettingsBuilder.PlaybackSpeedChoices.VERY_SLOW
Specifies very slow playback speed (quarter of record speed)
|
Modifier and Type | Method and Description |
---|---|
MovieSettingsBuilder.PlaybackSpeedChoices |
MovieSettingsBuilder.playbackSpeed()
Returns the speed at which the recorded movie is played back.
|
static MovieSettingsBuilder.PlaybackSpeedChoices |
MovieSettingsBuilder.PlaybackSpeedChoices.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MovieSettingsBuilder.PlaybackSpeedChoices |
MovieSettingsBuilder.PlaybackSpeedChoices.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MovieSettingsBuilder.PlaybackSpeedChoices[] |
MovieSettingsBuilder.PlaybackSpeedChoices.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MovieSettingsBuilder.setPlaybackSpeed(MovieSettingsBuilder.PlaybackSpeedChoices playbackSpeed)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.