public interface MovieSettingsBuilder extends Builder
MovieManager.createMovieSettingsBuilder()
Property | Value |
---|---|
CaptureArea | Graphics |
FramesPerSecond | 10 |
PlaybackSpeed | AsRecorded |
Modifier and Type | Interface and Description |
---|---|
static class |
MovieSettingsBuilder.CaptureAreaChoices
Indicates the are being recorded in the movie.
|
static class |
MovieSettingsBuilder.PlaybackSpeedChoices
Indicates the playback speed of the movie.
|
Modifier and Type | Method and Description |
---|---|
MovieSettingsBuilder.CaptureAreaChoices |
captureArea()
Returns the area captured for movie creation.
|
String |
codecFourcc()
Returns the Codec that is used to create the movie.
|
int |
framesPerSecond()
Returns the frames per second for the movie.
|
MovieSettingsBuilder.PlaybackSpeedChoices |
playbackSpeed()
Returns the speed at which the recorded movie is played back.
|
void |
setCaptureArea(MovieSettingsBuilder.CaptureAreaChoices captureArea)
License requirements: None. |
void |
setCodecFourcc(String codecFourcc)
License requirements: None. |
void |
setFramesPerSecond(int framesPerSecond)
License requirements: None. |
void |
setPlaybackSpeed(MovieSettingsBuilder.PlaybackSpeedChoices playbackSpeed)
License requirements: None. |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
MovieSettingsBuilder.CaptureAreaChoices captureArea() throws NXException, RemoteException
NXException
RemoteException
void setCaptureArea(MovieSettingsBuilder.CaptureAreaChoices captureArea) throws NXException, RemoteException
captureArea
- NXException
RemoteException
int framesPerSecond() throws NXException, RemoteException
NXException
RemoteException
void setFramesPerSecond(int framesPerSecond) throws NXException, RemoteException
framesPerSecond
- NXException
RemoteException
MovieSettingsBuilder.PlaybackSpeedChoices playbackSpeed() throws NXException, RemoteException
NXException
RemoteException
void setPlaybackSpeed(MovieSettingsBuilder.PlaybackSpeedChoices playbackSpeed) throws NXException, RemoteException
playbackSpeed
- NXException
RemoteException
String codecFourcc() throws NXException, RemoteException
NXException
RemoteException
void setCodecFourcc(String codecFourcc) throws NXException, RemoteException
codecFourcc
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.