public static class TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC
Motion type: Automatic to start of engage.
|
static int |
_AXIAL_THEN_RADIAL
Motion type: Axial then radial to start of engage.
|
static int |
_CLEAR_AXIAL_THEN_DIRECT
Motion type: Axial to clearance plane then direct to start of engage.
|
static int |
_CLEAR_RADIAL_THEN_DIRECT
Motion type: Radial to clearance plane then direct to start of engage.
|
static int |
_DIRECT
Motion type: Direct to start of engage.
|
static int |
_RADIAL_THEN_AXIAL
Motion type: Radial then axial to start of engage.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
AUTOMATIC
Motion type: Automatic to start of engage.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
AXIAL_THEN_RADIAL
Motion type: Axial then radial to start of engage.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
CLEAR_AXIAL_THEN_DIRECT
Motion type: Axial to clearance plane then direct to start of engage.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
CLEAR_RADIAL_THEN_DIRECT
Motion type: Radial to clearance plane then direct to start of engage.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
DIRECT
Motion type: Direct to start of engage.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
RADIAL_THEN_AXIAL
Motion type: Radial then axial to start of engage.
|
Modifier and Type | Method and Description |
---|---|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes AUTOMATIC
public static final TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes DIRECT
public static final TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes RADIAL_THEN_AXIAL
public static final TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes AXIAL_THEN_RADIAL
public static final TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes CLEAR_RADIAL_THEN_DIRECT
public static final TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes CLEAR_AXIAL_THEN_DIRECT
public static final int _AUTOMATIC
public static final int _DIRECT
public static final int _RADIAL_THEN_AXIAL
public static final int _AXIAL_THEN_RADIAL
public static final int _CLEAR_RADIAL_THEN_DIRECT
public static final int _CLEAR_AXIAL_THEN_DIRECT
public static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes valueOf(int value)
public static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes valueOf(String name)
public static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.