Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes.AUTOMATIC
Motion type: Automatic to start of engage.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes.AXIAL_THEN_RADIAL
Motion type: Axial then radial to start of engage.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes.CLEAR_AXIAL_THEN_DIRECT
Motion type: Axial to clearance plane then direct to start of engage.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes.CLEAR_RADIAL_THEN_DIRECT
Motion type: Radial to clearance plane then direct to start of engage.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes.DIRECT
Motion type: Direct to start of engage.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes.RADIAL_THEN_AXIAL
Motion type: Radial then axial to start of engage.
|
Modifier and Type | Method and Description |
---|---|
TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
TurnAvoidanceStartOfEngageBuilder.startOfEngageMotionType()
Returns the start of engage motion type
License requirements: None. |
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes |
TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes[] |
TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnAvoidanceStartOfEngageBuilder.setStartOfEngageMotionType(TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes startOfEngageMotionType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.