public static class InPathEventDataBuilder.LocationMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DISTANCE_FROM_END
Distance From End
|
static int |
_DISTANCE_FROM_START
Distance From Start
|
static int |
_SPECIFY
Uses Point to define the InPath Events Location
|
static InPathEventDataBuilder.LocationMethod |
DISTANCE_FROM_END
Distance From End
|
static InPathEventDataBuilder.LocationMethod |
DISTANCE_FROM_START
Distance From Start
|
static InPathEventDataBuilder.LocationMethod |
SPECIFY
Uses Point to define the InPath Events Location
|
Modifier and Type | Method and Description |
---|---|
static InPathEventDataBuilder.LocationMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InPathEventDataBuilder.LocationMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InPathEventDataBuilder.LocationMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final InPathEventDataBuilder.LocationMethod SPECIFY
public static final InPathEventDataBuilder.LocationMethod DISTANCE_FROM_START
public static final InPathEventDataBuilder.LocationMethod DISTANCE_FROM_END
public static final int _SPECIFY
public static final int _DISTANCE_FROM_START
public static final int _DISTANCE_FROM_END
public static InPathEventDataBuilder.LocationMethod valueOf(int value)
public static InPathEventDataBuilder.LocationMethod valueOf(String name)
public static InPathEventDataBuilder.LocationMethod[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.