Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InPathEventDataBuilder.LocationMethod |
InPathEventDataBuilder.LocationMethod.DISTANCE_FROM_END
Distance From End
|
static InPathEventDataBuilder.LocationMethod |
InPathEventDataBuilder.LocationMethod.DISTANCE_FROM_START
Distance From Start
|
static InPathEventDataBuilder.LocationMethod |
InPathEventDataBuilder.LocationMethod.SPECIFY
Uses Point to define the InPath Events Location
|
Modifier and Type | Method and Description |
---|---|
InPathEventDataBuilder.LocationMethod |
InPathEventDataBuilder.method()
Returns the Inpath Events Location method
License requirements: cam_base ("CAM BASE") . |
static InPathEventDataBuilder.LocationMethod |
InPathEventDataBuilder.LocationMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InPathEventDataBuilder.LocationMethod |
InPathEventDataBuilder.LocationMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InPathEventDataBuilder.LocationMethod[] |
InPathEventDataBuilder.LocationMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InPathEventDataBuilder.setMethod(InPathEventDataBuilder.LocationMethod method)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.