Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Interface and Description |
---|---|
interface |
TBSShapeRestrictArea
Represents the restrictions of the design variable in Shape optimization
To create or edit an instance of this class, use TBSShapeRestrictAreaBuilder Created in NX8.5.0 |
interface |
TBSTopologyRestrictArea
Represents the restrictions of the design variable in topology optimization
To create or edit an instance of this class, use TBSTopologyRestrictAreaBuilder Created in NX8.0.0 |
Modifier and Type | Method and Description |
---|---|
TBSRestrictArea |
TBSRestrictAreaCollection.findObject(String name)
Finds a restrict area with the specified name within an optimization solution
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.