public static class TBSCastCondition.MiddlePlaneType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC
Automatica determinaton of the central plane
|
static int |
_AUTOMATIC_TIGHT
No holes are generated in the central plane
|
static int |
_NONE
No definition of a central plane
|
static int |
_POINT
A point within the central plane from which the deformation vector is positioned perpendicular to
|
static int |
_STAMP
The element group is demolded keeping a stampable structure
|
static int |
_SURFACE
The elements are demolded at the actual surface of the restrict area
|
static TBSCastCondition.MiddlePlaneType |
AUTOMATIC
Automatica determinaton of the central plane
|
static TBSCastCondition.MiddlePlaneType |
AUTOMATIC_TIGHT
No holes are generated in the central plane
|
static TBSCastCondition.MiddlePlaneType |
NONE
No definition of a central plane
|
static TBSCastCondition.MiddlePlaneType |
POINT
A point within the central plane from which the deformation vector is positioned perpendicular to
|
static TBSCastCondition.MiddlePlaneType |
STAMP
The element group is demolded keeping a stampable structure
|
static TBSCastCondition.MiddlePlaneType |
SURFACE
The elements are demolded at the actual surface of the restrict area
|
Modifier and Type | Method and Description |
---|---|
static TBSCastCondition.MiddlePlaneType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSCastCondition.MiddlePlaneType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSCastCondition.MiddlePlaneType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TBSCastCondition.MiddlePlaneType NONE
public static final TBSCastCondition.MiddlePlaneType AUTOMATIC
public static final TBSCastCondition.MiddlePlaneType AUTOMATIC_TIGHT
public static final TBSCastCondition.MiddlePlaneType POINT
public static final TBSCastCondition.MiddlePlaneType SURFACE
public static final TBSCastCondition.MiddlePlaneType STAMP
public static final int _NONE
public static final int _AUTOMATIC
public static final int _AUTOMATIC_TIGHT
public static final int _POINT
public static final int _SURFACE
public static final int _STAMP
public static TBSCastCondition.MiddlePlaneType valueOf(int value)
public static TBSCastCondition.MiddlePlaneType valueOf(String name)
public static TBSCastCondition.MiddlePlaneType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.