public static class ElementQualitySetting.LimitValue extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ERROR_LIMIT_ONLY
Only error criteria value could be defined
|
static int |
_WARNING_AND_ERROR_LIMIT
Both warning and error criteria value could be defined
|
static ElementQualitySetting.LimitValue |
ERROR_LIMIT_ONLY
Only error criteria value could be defined
|
static ElementQualitySetting.LimitValue |
WARNING_AND_ERROR_LIMIT
Both warning and error criteria value could be defined
|
Modifier and Type | Method and Description |
---|---|
static ElementQualitySetting.LimitValue |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElementQualitySetting.LimitValue |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElementQualitySetting.LimitValue[] |
values()
Returns an array that contains the values for this enum.
|
public static final ElementQualitySetting.LimitValue WARNING_AND_ERROR_LIMIT
public static final ElementQualitySetting.LimitValue ERROR_LIMIT_ONLY
public static final int _WARNING_AND_ERROR_LIMIT
public static final int _ERROR_LIMIT_ONLY
public static ElementQualitySetting.LimitValue valueOf(int value)
public static ElementQualitySetting.LimitValue valueOf(String name)
public static ElementQualitySetting.LimitValue[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.