Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Result.DeformationScale |
Result.DeformationScale.ABSOLUTE |
Result.DeformationScale |
Result.DeformationParameters.deformationScale
Deprecated.
|
static Result.DeformationScale |
Result.DeformationScale.MODEL |
Modifier and Type | Method and Description |
---|---|
Result.DeformationScale |
DeformationParameters.deformationType()
Returns the type of scale used for deforming the model
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static Result.DeformationScale |
Result.DeformationScale.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Result.DeformationScale |
Result.DeformationScale.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Result.DeformationScale[] |
Result.DeformationScale.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DeformationParameters.setDeformationType(Result.DeformationScale unit)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Constructor and Description |
---|
DeformationParameters(int loadCaseIndexInitial,
int iterationIndexInitial,
Result.Type typeInitial,
Result.Complex complexInitial,
double phaseAngleInitial,
Result.DeformationScale deformationScaleInitial,
double absoluteScaleValueInitial,
double modelPercentScaleValueInitial)
Deprecated.
Constructor for the DeformationParameters object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.